System Remote Commands

System Remote Commands ClosedSetup

SCPI Error Queue

Retrieve All Entries In The Queue

Number of Entries In The Queue

Retrieve Next Entry

Retrieve Next Entry Code

Retrieve All Error Codes

Clear Error History

Message in the Message Queue

List installed Software Options

Display Refresh State

Display State

Display Annotation State

Lock the Front-Panel Keys

Lock Workstation

List SCPI Commands

Instrument start time

SCPI Version Query

Attenuator Bypass History

Controller BIOS

The commands in this section are remote commands only and have no front-panel key / GUI equivalent.

SCPI Error Queue

The signal generator instrument provides the remote operation error queue as defined in IEEE SCPI standard version 1999.

Items in the SCPI Error queue are from remote operations. These are separate from the errors generated from front panel operations (see Message queue for front panel operations errors).

There is a separate SCPI Error queue for each I/O session. Boot-up instrument messages are handled differently. These messages are placed into the error queue of the first I/O session.

*CLS clears all entries in the queue. See *CLS for more information.

Retrieve All Entries In The Queue

Remote command only.

Queries the SCPI Error queue for all unread items and removes them from the queue. The response is a comma separated list of number, string pairs in FIFO order. If the queue is empty, the response is 0,"".

SCPI Command

:SYSTem:ERRor:ALL?

SCPI Example

SYST:ERR:ALL?

Notes When the SCPI Error queue is empty, 0,"" is returned.
Preset N/A

State Saved

No

Initial S/W Revision

A.01.00

Number of Entries In The Queue

Remote command only.

Queries the SCPI Error queue for the number of unread items. As errors and events may occur at any time, more items may be present in the queue at the time it is actually read.

SCPI Command

:SYSTem:ERRor:COUNt?

SCPI Example

SYST:ERR:COUN?

Notes If the queue is empty, 0 is returned.
Preset N/A

State Saved

No

Initial S/W Revision

A.01.00

Retrieve Next Entry

Remote command only.

Queries the SCPI Error queue for the next item and removes it from the queue. The response returns the full queue item consisting of an integer and a string. When the queue is empty, 0,"No error" is returned.

SCPI Command

:SYSTem:ERRor[:NEXT]?

SCPI Example

SYST:ERR?

Notes If the queue is empty, 0,"No error" is returned.

State Saved

No

Initial S/W Revision

A.01.00

Retrieve Next Entry Code

Remote command only.

Queries the SCPI Error queue for the next item and removes this item from the queue. The response returns only the error code number omitting the string. When the queue is empty, 0 is returned.

SCPI Command

:SYSTem:ERRor:CODe[:NEXT]?

SCPI Example

SYST:ERR:COD?

Notes If the queue is empty, 0 is returned.
Preset N/A

State Saved

No

Initial S/W Revision

A.01.00

Retrieve All Error Codes

Remote command only.

Query Only.

Returns all entries in the error queue and then clears the queue. The response returns only the error code numbers, omitting the string.

SCPI Command

:SYSTem:ERRor:CODE:ALL?

SCPI Example

:SYST:ERR:CODE:ALL?

Notes

When the queue is empty, returns 0.

State Saved

No

Initial S/W Revision

A.20.00

Clear Error History

Remote command only

Clears the GUI and SCPI error queue. There is no query form for the command.

SCPI Command

:SYSTem:ERRor:HISTory:CLEar

SCPI Example

SYST:ERR:HIST:CLE

State Saved

No

Initial S/W Revision

A.20.00

Message in the Message Queue

Remote command only.

Queries the Message queue and returns the first message which has not been queried/read from this queue. Subsequent query returns the next unread message from the queue, and so on.

SCPI Command

:SYSTem:NOTification?

SCPI Example

:SYST:NOT?

Notes

The response is a comma separated value that consists of:

  • a string representing the timestamp of the message with the format "MM/DD/YYYY<space>HH:MM<space><AM or PM>" in instrument local time. "HH" is 12-hour clock. "<AM or PM>" shows before or after midday by "AM" or "PM".

  • an enum representing the type of message with the enumerations shown below.

    • NONE - Indicates that no unread message is left in the Message queue for the query.

    • INFormation

    • WARNing

    • ERRor

  • a string representing the message.

When all messages have been read from the queue, further queries return: "",NONE,""
Messages related only to the User Interface, such as "Local Operation Resumed", are not returned by this command.
This command only queries and returns the message from the Message queue but does not alter the contents of the Message queue.

Initial S/W Revision

A.16.20

List installed Software Options

Remote command only.

This query returns a comma-separated list of installed software application options. This differs from the output for *OPT? in that the *OPT? lists the installed hardware options.

SCPI Command

:DIAGnostic[:CPU]:INFormation:OPTions?

SCPI Example

:DIAG:INF:OPT?

State Saved

No

Initial S/W Revision

A.01.00

Lock the Front-Panel Keys

Remote command only.

Disables the instrument keyboard to prevent local input when the instrument is controlled remotely. Annunciation showing a "K" for "Klock" (keyboard lock) alerts the local user that the keyboard is locked. Klock is similar to the GPIB Local Lockout function; namely that no front-panel keys are active with the exception of the Power Standby key. (The instrument is allowed to be turned-off if Klock is ON.) The Klock command is used in remote control situations where Local Lockout cannot be used.

Although primary intent of Klock is to lock-out the front panel, it will lock-out externally connected keyboards through USB. Klock has no effect on externally connected pointing devices (mice).

The front panel ‘Local’ key (Cancel/Esc) has no effect if Klock is ON.

SCPI Command

:SYSTem:KLOCk OFF|ON|0|1

:SYSTem:KLOCk?

SCPI Example

:SYST:KLOC ON

Notes

Keyboard lock remains in effect until turned-off or the instrument is power-cycled

Preset

Initialized to OFF at startup, unaffected by Preset

State Saved

No

Initial S/W Revision

A.01.00

Display Refresh State

Remote command only.

Enables or disables active updates for the instrument’s display when the instrument is remotely controlled. When On, the performance (speed) of the remote operation may be degraded. If the instrument is not in LOCAL LOCKOUT, pressing the ESC/Local key on the instrument’s front panel will set the display to On and resume display updates.

SCPI Command

:DISPlay:REMote ON|OFF|1|0

:DISPlay:REMote?

SCPI Example

DISP:REM OFF

DISP:REM?

Notes

Pressing the front panel Local key sets the state to On.

Preset

Not affected by Preset, not part of Persistent State. Always ON immediately after the instrument is booted.

State Saved

No

Initial S/W Revision

A.13.00

Display State

Remote command only.

Turns the display state of the screen On or Off. If the instrument is not in LOCAL LOCKOUT, pressing the ESC or Local key on the instrument’s front panel will set the display to On.

SCPI Command

:DISPlay[:WINDow][:STATe]

:DISPlay[:WINDow][:STATe]?

SCPI Example

DISP OFF

DISP?

Couplings

When Display State is turned OFF/ON, Display Refresh State will also be set to OFF/ON.

Preset

ON

State Saved

No

Initial S/W Revision

A.18.01

Display Annotation State

Remote command only

Sets whether the Power and Frequency (CW) values are displayed on the Home screen or hidden.

SCPI Command

:DISPlay:ANNotation ON|OFF|1|0

:DISPlay:ANNotation?

SCPI Example

DISP:ANN OFF

DISP:ANN?

Preset

ON

State Saved

Y

Initial S/W Revision

A.20.00

Lock Workstation

Remote command only.

Performs the same functionality as the Win+L function or the "Lock" function on the CTL-ALT-DEL screen in Windows. 

When this command is executed, the computer is immediately locked. The initial login screen appears; no one can access the computer at this point unless they have an account and know the account’s password.

SCPI Command

:SYSTem:LWSTation

SCPI Example

:SYST:LWST

Notes

The lock remains in effect until someone logs in

State Saved

No

Initial S/W Revision

A.01.00

List SCPI Commands

Remote command only.

Outputs a list of the valid SCPI commands for the currently selected Mode.

SCPI Command

:SYSTem:HELP:HEADers?

SCPI Example

:SYST:HELP:HEAD?

Notes

The output is an IEEE Block format with each command separated with the New-Line character (hex 0x0A)

Initial S/W Revision

A.01.00

Instrument start time

Remote command only.

Determines the instrument application start time.

SCPI Command

:SYSTem:METRics:STIMe?

SCPI Example

:SYST:METR:STIM?

Notes

The return value is a string with the format "YYYY-MM-DD<space>HH:MM:SS", in instrument local time.

Initial S/W Revision

A.01.00

SCPI Version Query

Remote command only.

Returns the SCPI version number with which the instrument complies. The SCPI industry standard changes regularly. This command indicates the version used when the instrument SCPI commands were defined.

SCPI Command

:SYSTem:VERSion?

SCPI Example

:SYST:VERS?

Initial S/W Revision

A.01.00

Attenuator Bypass History

Remote command only.

Query only

Returns the cumulative number of times that the attenuator bypass has been switched. The subopcode indicates the channel being queried.

SCPI Command

:DIAGnostic[:CPU]:INFormation:CCOunt:ATTenuator[1]|2:BYPass?

SCPI Example

:DIAG:INF:CCO:ATT:BYP?

Initial S/W Revision

A.01.00

Controller BIOS

Remote command only.

Query only.

Returns the CPU’s BIOS version in the format provided by the CPU manufacturer.

SCPI Command

:DIAGnostic[:CPU]:BIOS:VERSion?

SCPI Example

:DIAG:BIOS:VERS?

Notes

Return value is a string of the BIOS version in the format provided by the controller’s manufacturer.

Initial S/W Revision

A.09.00